Loading...
Selected products added to your list. To view the list, Click here

Leviton OPT-X™ SJZ Fiber Cable and Assemblies Now Available

Trunk assemblies support EMEA data center managers with two performance levels

Glenrothes, UK, July 11, 2023 – Leviton today announced that the new OPT-X™ SJZ sub-jacketed fiber cable and associated pre-terminated fiber trunks are now available to support data centers and network managers throughout Europe, the Middle East and Africa. The addition of SJZ cables and trunk assemblies complements the popular OPT-X SJP sub-jacketed plenum-rated solutions in North America. Both SJZ and SJP make up the SJX global family of loose-tube cable and trunk assemblies, with fire ratings that cover all regions around the world.

SJZ cabling features sub-jacketed fiber groups that qualify as a rated cable for individual routing paths, giving network managers more options with breakouts in racks, cabinets and cable management routing. The cables are rated EuroClass B2ca, s1a d1 a1 for LSZH installations, and OFNR-FT4-ST1 for riser installations. Available in 12- to 144-count fiber constructions, SJZ cable is optimized for use in indoor installations and, as part of a Made-to-Order Trunk Cable Assembly, is available with single-mode and OM3, OM4 and OM5 multimode fibers.

SJZ pre-terminated trunk assemblies are available in two performance levels: OPT-X Unity SJZ Trunks for ultra-low-loss performance channels and OPT-X Engage SJZ Trunks for low-loss performance channels. These offerings support greater distances and multiple connection points while staying within IEEE low-loss limits. The trunk assemblies are part of Leviton OPT-X global end-to-end fiber systems, available to customers worldwide.

"B2ca trunks now complement our fiber assembly range and ensures that all fiber assemblies have the highest possible Euroclass rating in EMEA," said Michael Lawrence, product manager for Leviton Network Solutions EMEA. "As part of a global solution, SJZ allows multinational organizations to use consistent project specifications across regions. Additionally, we’ve built SJZ cable for easier installations, with a tight bend radius and no preferential bend direction."

For more information about Leviton's Made-To-Order fiber trunks, visit leviton.com/ns/emea/mto.

###

About Leviton Network Solutions
Leviton Network Solutions is a single-source global manufacturer of copper and fiber cabling systems. Leviton solutions are used in data centers, businesses, schools, hospitals, government facilities and commercial mixed-use markets around the world. All Leviton products are engineered to exacting standards, offer industry-leading performance and are backed by the industry’s best service and support. IT management, builders, contractors, and other industry professionals consistently rank Leviton products as the most preferred brand in the industry. We can expand your network possibilities. Learn more at www.leviton.com/ns or www.twitter.com/LevitonNS. European customers can visit leviton.com/ns/emea or twitter.com/LevitonNS_EU.