Wired Companion Device Features

Not a Stand-Alone Device
This device can only be used in 3-way or more installations and requires a primary Decora Smart® (Wi-Fi®, Z-Wave®, HomeKit or Zigbee®) or Decora Digital dimmer or fan speed control to operate.
Brightness/Fan Speed Display
Lights up to display the brightness or fan speed level. Tracks the main dimmer or fan speed control.
Rocker Switch
Separate ON/OFF switch allows the light or fan speed setting to remain at set level
Brightness/Fan Speed Control Bar
Press bar up or down to adjust brightness or fan speed level.
Locator LED
Illuminates when load is off, making it easy to locate in the dark.
Not a Stand-Alone Device
This device can only be used in 3-way or more installations and requires a primary Decora Smart® (Wi-Fi®, Z-Wave®, HomeKit or Zigbee®) or Decora Digital switch, dimmer or fan speed control to operate.
Rocker Switch
Tap the top to manually turn your lights or fan on, tap the bottom to turn them off.
Locator LED (DD0SR-DLZ only)
Illuminates when load is off making it easy to locate in the dark.
Explore our Wired Companion Devices
Choosing the Right Companion Device
Companion devices are intended to be used in 3-way or multi-location applications. They must be paired with a primary dimmer, switch or fan speed control in order to function. The chart below identifies companion devices and which primary devices they can be used with.
Companion Dimmer, Use With: | Wi-Fi | Z-Wave Plus | ZigBee | Decora Digital |
Primary Dimmer: | D26HD DWVAA | DZ6HD DZPD3 | DG6HD DG3HL | DDL06-1 DDM06 DDMX1 DDL06-B DDE06 DD710 |
Primary Sensor: | D2MSD | - | - | - |
Primary Fan Speed Control: | DW4SF | ZW4SF | - | DDF01 |
Companion Switch, Use With: | Wi-Fi | Z-Wave Plus | ZigBee | Decora Digital |
Primary Switch: | D215S D2SCS | DZ15S | DG15S | DDS15 |
Primary Dimmer (On/Off Only): | D26HD DWVAA | DZ6HD | DG6HD | DDL06-1 DDM06 DDMX1 DDL06-B DDE06 DD710 |
Primary Sensor: | D2MSD | - | - | - |
Primary Fan Speed Control: | ZW4SF | - | - | DDF01 |
Featured Videos
DD00R Frequently Asked Questions
No. This is a companion device intended for 3-way or more applications only and must be used with a Decora Smart dimmer, Decora Smart fan speed control, Decora Digital dimmer or Decora Digital fan speed control.
Single pole means controlling one or more lighting fixtures from a single location. Multi-location is the ability to control one or more lighting fixtures from two or more locations.
The primary dimmer will be used in the main location and the DD00R-DLZ dimmer companion(s) can be used in up to 4 additional locations. An example would be a large great room where there are several locations in which you can control the same lights.
Yes, a neutral wire is required to install the DD00R-DLZ dimmer companion. Neutral wires are typically two or more white wires in an electrical box. If you are unsure consult an electrician.
The maximum wire length from the primary dimmer to the dimmer companion(s) cannot exceed 300 Ft (90m).
DD0SR-DLZ Frequently Asked Questions
No. This is a companion device intended for 3-way or more applications to provide on/off switching and must be used with Leviton’s Decora Smart or Decora Digital primary switches, dimmers, or fan speed controls.
Single pole means controlling one or more lighting fixtures from a single location. Multi-location is the ability to control one or more lighting fixtures from two or more locations.
The primary device will be used in the main location and the DD0SR-DLZ switch companion(s) can be used in up to 4 additional locations. An example would be a large great room where there are several locations in which you can control the same lights.
Yes, a neutral wire is required to install the DD0SR-DLZ switch companion. Neutral wires are typically two or more white wires in an electrical box. If you are unsure consult an electrician.
The maximum wire length from the primary switch to the switch companion(s) cannot exceed 300 Ft (90m).
DD0SR-1Z Frequently Asked Questions
No. This is a companion device intended for 3-way or more applications to provide on/off switching and must be used with Leviton’s Decora Smart or Decora Digital primary switches, dimmers, or fan speed controls.
Single pole means controlling one or more lighting fixtures from a single location. Multi-location is the ability to control one or more lighting fixtures from two or more locations.
The primary device will be used in the main location and the DD0SR-1Z switch companion(s) can be used in up to 9 additional locations. An example would be a large great room where there are several locations in which you can control the same lights.
Although a neutral wire is preferred, it is not required. There are alternative wiring methods that can be used to install the DD0SR-1Z when a neutral wire is not present. Please see the product instruction sheet for details.
The maximum wire length from the primary switch to the switch companion(s) cannot exceed 300 Ft (90m).
Resources
How Can We Help?
Do you have questions about our Wired Companion Devices?