Whatever your application, Leviton’s line up of GFCI receptacles offers a wide variety of options
Electrical safety is a priority in every home. Leviton safety devices help protect people and property all while meeting or exceeding National Electric Code® (NEC®) standards. Our extensive line of SmartlockPro® Self-Test GFCI (Ground-Fault Circuit Interrupter) Receptacles includes: Lever Edge Standard, Weather-Resistant, Combination GFCI/USB, Combination GFCI/Switch, Guide Light, Audible Alert, Smart GFCI, Dual Function AFCI/GFCI and Blank Face. All of our GFCI receptacles and circuit breakers are engineered to help protect people from the hazards of electric shock and electrocution by interrupting power if a ground-fault is detected. GFCI outlets are required by the NEC® for areas around the home within a close proximity to a water source, such as kitchens, bathrooms, laundry rooms, basements, garages/carports and outdoor areas such as pools, spas, decks and patios.
Explore Our GFCI Products
Superior GFCI Protection. Advanced Technology. Only from Leviton.

Leviton Patented Reset Lockout
Prevents reset if GFCI is damaged and cannot respond to a ground-fault
Terminals Withstand High Torque
Tolerates high-torque power tool installation and prevents wire pullout
Tamper-Resistant Shutters
Meets NEC® 406.12 requirement by blocking access to the contacts unless a two- or three-prong plug is inserted
Back and Side Wire
Two convenient wiring options; the external clamp also provides visual indication of proper wire seating
Status Indicator Light
Red and green LED indications provide simple, intuitive feedback on power and protection status as well as correct wiring
Standard Self-Ground Clip
Grounds the device in grounded metal box installations
Only 1.026” Protrusion into Wallbox
Takes up to 25% less space in the wallbox vs. other GFCIs for easier installation
Exceeds UL Safety Standards
Ground-fault and dual-function circuit breakers exceed UL safety standards.
Hydraulic-Magnetic Trip Technology
Hydraulic-magnetic trip technology ensures precise tripping even in extreme temperature ranges.
Easy-to-Read Diagnostics
Easy-to-read LEDs help communicate trip condition and type of fault.
Smart-Enabled Available
Optional Wi-Fi® or Ethernet connectivity with the My Leviton app.
Learn more »Leviton’s patented reset/lockout feature on all of our SmartlockPro® GFCI receptacles prevent reset of the device if for any reason it is unable to respond to a ground-fault or if it is not wired correctly. Additionally, all of our GFCIs conduct an automatic self-test which improves safety by regularly confirming they can respond to a ground-fault.
Where to Install
Slim Profile for Easier Installation
Leviton SmartlockPro® outlets feature the slimmest profile on the market for easy installation, every time.
What are Ground-Faults?
- Ground-faults occur when a current flows along an unintended path, such as through water or a person.
- Since their invention in the 1970s, GFCIs have played an important role in helping to reduce the occurrence of shocks and electrocutions.


How are Leviton GFCI Circuit Breakers Different?
- GFCI and GFPE Circuit Breakers are available in standard or smart varieties which allow you to remotely monitor, update and trip your breaker from anywhere in the world with the MyLeviton app and feature the fastest installation on the market today.
Why Choose a Leviton GFCI?
- Protection without exception. Other manufacturers may allow their GFCI devices to be reset even after protection is permanently lost – taking advantage of UL exemptions and providing users with unprotected power. Why take chances?

Videos
The Leviton GFCI Portfolio
Learn more about our variety of GFCI outlets to meet any application.
Leviton GFCIs on Today’s Homeowner
Learn more about our Self-Test GFCI outlets from Danny Lipford.
Leviton Answer Series: GFCI Line-Load Reversal
What to do if your GFCI is not working. Common wiring mistakes.
Leviton Answer Series: Preventing Electrical Shock
Learn how to keep your family safe from electrical shock with Leviton GFCIs.
Leviton Presents: How to Install AFCI/GFCI Outlets
Learn how to wire and install our AFCI/GFCI outlets.
The Easy to Install GFCI
See why Leviton is the clear choice for your next DIY installation.
Leviton Answer Series: What To Do When Your GFCI Trips
What you can do when your GFCI trips and when it’s time to call an electrician.
GFCIs (Ground-Fault Circuit Interrupters) Frequently Asked Questions
If your GFCI does not reset after installation this is often the result of reversing the LINE and LOAD wires when installing. You can diagnose this when you flip the breaker to reconnect power and the indicator light is green while the GFCI will not allow you to reset. This can easily be addressed by correcting the wiring. Take a look at the back of the device you are installing to note which side is the LINE and which side is the LOAD and attach the wires accordingly. Simply connecting the wires exactly the same as they are on the older device may cause this reversal. Leviton GFCIs protect against being reset unless they are properly wired, operating correctly, and connected to power.
The GFCI has internal parts that automatically conduct a test on regular intervals to ensure that the GFCI sensing and trip capabilities are intact. If the self-test sequence determines there is a potential loss of protection the GFCI will need to take specific actions such as tripping or providing an indication to alert end users.
The terms are interchangeable and mean the same thing. UL uses the term auto-monitoring and many of the GFCI manufacturers use the term self-test.
All the GFCIs manufactured after June 29, 2015 must include the auto-monitoring and many of the GFCI manufacturers use the term self-test.
No, as long as the outlet is not worn and you have conducted the manual test to ensure it is providing protected power. If you are doing a renovation or are looking to upgrade your older GFCIs, the self-test models do add an additional layer of protection.
Only the Leviton Audible GFCIs provide audible indication. All other wallbox mounted GFCIs provide visual indication only.
The only way to tell is to press the "test" button and then the "reset" button. If the GFCI blinks RED once it is a self-test model. If the LED turns immediately to GREEN, it is a non-self-test model.
Yes, you should manually test your GFCIs on a monthly basis.
If the Leviton self-test has conducted a self-test and everything has checked out OK the indicator light will be green. If the indicator light is either not on or red you should conduct a manual test immediately. You can always conduct a manual TEST and RESET sequence to confirm the GFCI is functioning properly.
Resources
How Can We Help?
Do you have questions about our GFCIs?